Останні записи
Antimagnetic castors for the MRI scanner
A MRI generates strong magnetic fields and alternating magnetic fields. This makes special demands on the scanner and all its components, as well as other objects in the room. Castors, for example, must also have certain properties if they are to be used in conjunction with MRI scanners.
CAD: Computer Aided Design
The acronym CAD stands for Computer Aided Design. This means creating product graphics using a computer program. Both two and three dimensional drawings can be produced.
What factors influence the swivel resistance?
The swivel resistance of castors and wheels influences the manoeuvrability of a device.
Найпопулярніші технічні терміни
Wheels and castors
Wheels and castors are available in a variety of different designs. The function and quality of a castor or wheel depends on both the overall concept and the individual details.
Chemical resistance of castors and wheels
If castors or wheels are likely to come into contact with aggressive substances, their chemical resistance must be taken into account when selecting the right product.
CAD: Computer Aided Design
The acronym CAD stands for Computer Aided Design. This means creating product graphics using a computer program. Both two and three dimensional drawings can be produced.
Ваш вибір: %кількість% Товарів.
Товарів не знайдено.