C
9 Публикации в этой категории энциклопедииCAD: Computer Aided Design
The acronym CAD stands for Computer Aided Design. This means creating product graphics using a computer program. Both two and three dimensional drawings can be produced.
Castor and wheel requirements in intralogistics
The demands placed on castors and wheels in intralogistics are very high. The internal transport of goods needs to be safe, economical and efficient.
Castor housing
A castor basically consists of three important components: the wheel, the fitting and the castor housing. But what is the difference?
Castor swivel bearing
Manoeuvrability and flexibility are the most important advantages when using practically any castor. The swivel bearing or back bearing determines how easily and smoothly this works.
Castors for office chairs
The choice of castor for an office chair depends primarily on the type of floor:
Chemical resistance of castors and wheels
If castors or wheels are likely to come into contact with aggressive substances, their chemical resistance must be taken into account when selecting the right product.
Corrosion resistance of castors and wheels
Mobile devices are often used outdoors or in extreme conditions. In such cases, the corrosion resistance of the castors and wheels becomes important. The surfaces of the individual components must be appropriately treated to ensure that they are protected against corrosion.