F
7 Публикации в этой категории энциклопедииFind castors for tool trolleys
Tool trolleys are ideal for both professional craftspersons and DIY enthusiasts – for transporting large quantities of tools easily from one place to another.
Finding the right castors for hospital beds
Hospital beds are in constant use, have to be manoeuvred back and forth, sometimes through narrow aisles, and have to stand securely in the patient's room. In order to meet these requirements, hospital beds must be equipped with appropriate castors.
Fit care beds with easy-running, washable castors
Falling out of the care bed is a major risk that can never be completely eliminated. And bacteria and germs can spread incredibly quickly in care facilities. These factors also make great demands on the care bed castors.
Fitting elements for every type of use
The performance of a castor or wheel depends heavily on the optimum fitting. The type of fitting required is determined by the design of the equipment to which the castors are to be attached.
Foot protection for castors
The protection of personnel plays an important role in mobile castor applications. If feet should accidentally get under the wheels, serious injuries can occur.
Furniture castors: What must be taken into account?
Furniture castors are used in living rooms as well as in offices. The must meet different requirements depending on where they are used. These depend on the type of floor on which the castors are used, for example, and on the loads that have to be carried.