What requirements do industrial castors have to meet?
Applications for industrial castors
Whether at airports, in production facilities or in the army – industrial castors are used in many different areas. Castors for transport equipment, devices, and for heavy-duty use, are found in applications such as pallet trucks, disposal containers, mobile cranes and stairs, as well as for working platforms and many other applications. If you have any questions about which castor is suitable for your specific application, please contact us: We will find the ideal solution for you!
Properties of industrial castors
TENTE industrial castors have a very high load capacity of up to several thousand kilograms per castor. All of the components – from the tread to the housing – are made of robust materials that ensure good running characteristics as well as high corrosion resistance and wear resistance. Different versions are advantageous depending on the type of application. Different tread surfaces, bearing types and locking mechanisms are possible. Simulations and long-term tests are carried out on each castor to ensure permanently smooth operation.