Low-height caster to complement your design
One possible solution to this problem is to use sturdy casters with a low profile. Unlike traditional casters, which are often large and bulky, these casters can be placed unobtrusively under the store furniture. In this way, the appearance of the store furniture is not affected, and its aesthetics is preserved. Especially for modern store furniture, which often has a minimalist design, these casters are an ideal choice. The only drawback is that the casters must not be heavy-duty – and this is where TENTE comes in.


Our solution for you: Linea load
Our Linea load caster has the unique advantage of a small diameter combined with a high load capacity. With a wheel diameter of only 50 mm, this caster can carry a load of up to 100 kg, making it a particularly efficient and versatile product. The small diameter of the wheels provides more space to present and display the product on display.
In addition, Linea load can be seamlessly integrated with furniture to perfectly present the products for sale. The caster is available in different colors to complement the design of the furniture. If you need a special color, please contact our experts. We will create the perfect custom color for you.
Moreover, Linea load offers optimal maneuverability in an unlocked position. In other words, it can be moved easily and flexibly to change the position of store furniture and sales products quickly and easily. When locked, the brake lever ensures constant contact with the ground so that the caster does not move a millimeter from its position. This makes the TENTE caster a reliable and stable product that ensures a safe and firm stand.
Your advantages with Linea load
- Load capacity of 100 kg in the version with two wheels and low overall height to show and exhibit the product on display
- Perfect maneuverability thanks to precision ball bearings in the wheels
- Fixed locking system to keep everything in place
- Different colors to fit perfectly into your design
If you need more information or have any questions, please do not hesitate to contact us. We are always eager to help and consult you. If you need personalized advice or are looking for a customized solution for your specific needs, please do not hesitate to contact us. We have an experienced team of experts who will be happy to help you find the best solution for your needs. Please fill out the contact form below and we will get back to you as soon as possible. We look forward to hearing from you!


Why do casters with a low overall height show a lower load capacity?
Casters with a low overall height have a lower load capacity than casters with a greater overall height due to their design. This is because casters with a low overall height also have a smaller diameter. A smaller diameter results in a smaller contact area between the caster and the floor, which results in a higher load applied to the floor and the caster. As a result, the load capacity may be reduced.
What factors should you consider when choosing casters?
Choosing the right caster depends on several factors, such as the type of application, the load to be moved, and the type of floor on which the caster will be used. Important factors to consider when choosing the right caster are load capacity, diameter, floor condition, type of application, environment, and mounting. If you are unsure of which caster type or model is best, feel free to contact an expert to help you select the right caster.
How can store furniture casters influence customer movement and the shopping experience?
Store furniture casters can play an important role in shaping the shopping experience in retail stores. The right furniture casters can provide more flexibility, space optimization and easier movement.