Lexicon: T
Twin wheel caster
Twin wheel caster: robust and gentle on the floor
Thanks to high-quality materials such as plastic or sheet steel for the housing, the Twin wheel caster is very robust, but is gentle on the floor during use. A Twin wheel casterwith a soft tread is particularly suitable for sensitive floors such as tiles, parquet or laminate. Hard treads are better suited to soft floors such as carpet. As a variant, the double castor is also available in an electrically conductive version as well as washable and rustproof - a plus point for use in areas where hygiene regulations stipulate regular cleaning and disinfection.
TENTE Twin wheel caster not only meet high demands in terms of functionality and quality, but also in terms of design, including various colors and - as a special solution - an imprinted logo. Many of our products have already been awarded international design prizes.
The Twin wheel caster is very maneuverable thanks to the differential effect. This means that because the two wheels can also turn in opposite directions, the Twin wheel caster is easier to move and thus has an advantage over the simple furniture caster. This makes it ideal for applications where a lot of maneuvering is required. TENTE offers casters up to a load capacity of 12 tons (heavy duty casters).
Depending on requirements, various Twin wheel caster are available, such as those with different bearing arrangements - including a swivel bearing or a precision ball bearing - as well as variants with individually adjustable brakes. The latter are particularly suitable for sensitive areas of application that require smooth running and maximum running smoothness. These include laboratory equipment or hospital beds, for example.
If you have any questions about a Twin wheel caster or our other castors or wheels, please feel free to contact us. We will be happy to help you.