Lexicon: T
TENTE innovation – A combination of rigid and spring-loaded foot protection
The protection of personnel plays an important role in mobile caster applications. If feet should accidentally get under the wheels, serious injuries can occur. To prevent such injuries, casters can be equipped with a foot guard. This is screwed or welded onto the housing and is available in different sizes. The distance between the guard and the floor can also be selected.
One solution to these problems is to combine the rigid guard bars at the sides with springy aprons located in front of and behind the caster. This TENTE system solution provides optimal protection and prevents the problems that occur with the standard versions. Feet are protected from all potential angles of impact. These guards are also easy to replace or retrofit.
TENTE innovation – A combination of rigid and spring-loaded foot protection
One solution to these problems is to combine the rigid guard bars at the sides with springy aprons located in front of and behind the caster. This TENTE system solution provides optimal protection and prevents the problems that occur with the standard versions. Feet are protected from all potential angles of impact. These guards are also easy to replace or retrofit.