Lexicon: S
Store fixtures – easy maneuverability and a secure stand
Mobile shop building systems are used in supermarkets, shops and airports, for example. In supermarkets, fruit and vegetable display racks are pushed into the cool store every evening, for example, while discounted promotional merchandise in fashion stores is carefully positioned to promote sales. At airport bookshops, the most popular books are displayed in front of the entrance for passengers to pick up for inflight browsing. The mobility and maneuverability of these systems must be guaranteed at all times, as well as a secure stand when stationary. This requires special casters for store fixtures.
Often store fixtures have to be maneuvered in tight spaces. This requires swivel casters that can be moved in all directions. If inferior casters are used, more effort will be required to push the units. This will have a negative effect on the employee health. The casters should assure easy operating comfort and a high load capacity. It must always be possible to move store fixtures, not only when empty but also when fully loaded. When determining the necessary load capacity the total weight must be taken into account.
TENTE Linea combined twin wheels
The twin wheel casters of the TENTE Linea combined series have a robust caster lock. The wheel lock and directional lock are completely separate from one another in this caster. This ensures the caster can be fully locked, but also runs smoothly when the lock is released. The casters have a polyamide wheel body and a polyurethane tread. Electric conductive, stainless steel and washable versions are also available.
We will be happy to answer your questions about casters for shop fitting systems in detail – please contact our experienced team. If required, we are also at your disposal for developing innovative and individual special solutions.