Honored by the German Designer Club: TENTE Linea & Levina
TENTE casters prove their “Good Design”: The jury of the “Good Design” competition (www.ddc.de), which is organized annually by the Deutscher Designer Club, looks for the good and the extraordinary. In eight categories – including Product, but also Print, Digital, Future, Corporate and others - the interdisciplinary juries of experts select products for their "Good Design" and award gold, silver and bronze medals.
Various TENTE casters have already distinguished themselves as a results of their “good design”: The Linea hospital bed caster, winner of the silver medal, combines an exclusive design with the highest quality. This range of twin wheel casters made of plastic is versatile in use, easy to clean and can even be supplied with a particularly low overall height.
The Levina plastic caster, which combines the latest technology with a perfect design, was awarded the bronze medal in the competition. The robust housing and the use of high-quality plastic ensure a long service life. The Levina combines excellent running characteristics with first-class stability when stationary with a short, easy-to-operate brake pedal. The smooth surfaces are easy to clean, making the Levina ideal for use in the food industry.
An award-winning “Good Design”: High-flyer from TENTE
The Aviana twin wheel caster received an award for its “Good Design”. It is used on inflight trolleys and offers maximum ease and comfort above the clouds. Their quiet operating ensures that the cabin crew can move the trolleys safely through the tight spaces.
Bed casters from the 2940 series are particularly suitable for use in the medical sector. These simple twin wheel casters are not only durable and stable, they also withstand high impact load and are easy to move. This impressed the Deutscher Designer Club jury.