Heavy-duty casters
Special weights require special rollers: When massive scaffolding, huge overhead cranes or lead-heavy lift trucks have to be moved, strong performance is required without compromising precision and safety. Our "special unit" is there specifically for such applications: Our TENTE heavy-duty castors have been specially developed for transporting heavy loads.
The areas of application:
The areas of application of the heavy duty caster are very versatile and include, for example, the army or the transport of goods in factories. Other areas where the rollers are used are: - Airports - Ports - Manufacturing In these broad areas of application, there are many devices that can be equipped with the rollers. These include: - Working platforms - Mobile stairs - Mobile cranes - Transfer containers - Tugger trains.
Heavy duty casters make transporting heavy goods easy
Their solid construction with a heavy steel or stainless steel housing allows heavy duty casters to lift heavy weights. For example, they can withstand several hundred kilos or even up to twelve tons per roller. Despite these heavy loads, they are always easy to maneuver with precision, allowing you to move your heavy goods safely to their destination.
With the smooth-running heavy-duty casters, transporting large weights all at once becomes quite easy. The casters are manufactured with a high quality blue passivated surface finish that allows each of our casters to last a long time in use.
A heavy-duty castor for every situation
TENTE heavy-duty castors are available in various designs - for example as swivel castors with total lock or directional lock. These variants are particularly suitable for heavy vehicles that have to be maneuvered frequently and in all directions.
In addition, we also offer them as fixed castors, which provide more stability and a secure footing. Find the right castor for your application - TENTE's friendly service staff will be happy to advise you on any questions you may have about the material, properties and load capacity.
We are also happy to develop individual solutions for your special applications.
Proven safety thanks to continuous long-term testing
Safety comes first when transporting heavy weights, which is why heavy-duty rollers must be produced from absolutely reliable material. To ensure this, we constantly carry out stringent long-term tests. This involves simulating the load exerted by different weights - on different floors and under different influences.