Electromobility with Casters
The term electromobility is becoming increasingly important, not only due to constant developments in the automotive industry and other areas of drive technology, such as two-wheeled and public transport vehicles. But the subject of electric drives is pushing technology forward in the field of casters and wheels for a wide variety of applications. For example, the medical sector, hospitality industry and logistics sector all rely on electronically operated start-up aids.
Electromobility means drive efficiency for casters
Whenever heavy goods need to be moved, TENTE’s efficient E-Drive start-up aids lighten the load. Whether they are used in the health care sector, for example on hospital or care beds, or in logistics companies transporting goods, the drive modules on the casters reduce the risk of injury during loading and maneuvering. They dramatically reduce the physical effort that needs to be applied when handling heavy loads. They improve maneuvering around corners and in confined spaces. Electromobility in transport units improve health, safety and productivity in your company.
Starting up with electronic support
A DC gear motor forms the heart of TENTE drive systems. Its output is transferred to a drive wheel that enables the user to move heavy loads with much less physical effort. Moving the load, both forwards and backwards, is made easier, directional stability is improved, and the speed can be continuously controlled. Essentially, the E-Drive starting aids from TENTE consist of the following components: an electronic drive, control module, a manual control unit and a battery module. This system solution is also ideal for retrofitting existing transport units.