![](https://cdn.tente.com/media/79/76/32/1698405876/274-rollcontainer-desktop.jpg)
Lexicon: P
Particularly secure casters for roll containers in the fire service
Roll containers can be found in many places. Whether in the home office within your own four walls, in your office at work, in the first-aid room at the airport, or in the shopping centre – this practical storage furniture is extremely versatile.
Roll containers are used by the fire department to transport their equipment. When firefighters are called out, everything has to move fast, and everything has to be absolutely safe and secure. Therefore the casters on the roll containers must therefore be easy to move and lock in place, even under heavy load. We developed an innovative solution for this purpose: TENTE 349D. These rigid casters with a dynamic load capacity of up to 350 kg are equipped with an automatic locking system. This means the brake is always active and the caster is always locked. The container can only be moved when the handle is operated manually to release the brake. If the container threatens to roll away, the firefighters can simply let go of the handle and the locking system immediately takes effect again.
Discover TENTE’s high-quality casters for roll containers. If you need an individual solution, please contact us – we will develop innovative casters for your application!
Particularly reliable casters for roll containers in the fire service
Roll containers are used by the fire department to transport equipment. When firefighters are called out, everything has to move fast, but at the same time everything has to be absolutely secure. The casters on the roll containers must therefore be easy to move and lock in place, even under heavy load. We developed an innovative solution for this purpose: TENTE 349D. These fixed casters with a dynamic load capacity weighing up to 350 kg are equipped with an automatic locking system. This means that the brake is always active and the caster is always locked. The container can only be moved when the handle bar is operated manually to release the brake. If the container threatens to slip away, the firefighter can let go of the handle and the locking System is activated again.
Convince yourself of the high-quality of TENTE casters for roll containers. If you need an individual solution, please contact us – we will develop innovative casters for your application!