Lexicon Overview
The latest entries
MRI: Important factors in the selection of casters
Magnetic resonance imaging (MRI) is an imaging method used for medical diagnosis. It generates strong magnetic fields and alternating magnetic fields.
Factors influencing the swivel resistance
One type of resistance to which wheels and casters are subjected is the swivel resistance. This is the force that has to be applied to keep the rolling equipment in motion and to maneuver it.
The most read entries
Chemical resistance of casters & wheels
If casters or wheels are likely to come into contact with aggressive substances, their chemical resistance must be taken into account when selecting the right product.
Wheels and castors
Wheels and castors are available in a variety of different designs. The function and quality of a castor or wheel depends on both the overall concept and the individual details.
Other types of wheel bearings
To ensure that casters always run smoothly, they require a first-class wheel bearing.